This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: CCS/LAUNCHXL-F28379D

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMS320F28379D

Tool/software: Code Composer Studio

Can't upload code. It shows the following error...

C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code.  Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.

Please suggest corrections to be made.