Part Number: TIDM-SOMPLC-F28PLC83
Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDM-SOMPLC-F28PLC83
Hello,
The PLC Module in the document (System on Module for G3 Power Line Communication
(CENELEC Frequency Band)) has to be used with Docking station in fig8 correct?
hi Sumathi,
> For your previous questions ,
can we use this reference design to interface with SPI or UART? Yes you can
Do we require a G3-PLC data concentrator to connect to more number of nodes? you can use the same design to connect upto 32 nodes. For anything more the data concentrator is needed .
the below reference design can also be used
> In order to interface the G3-PLC solution from TI as mentioned in the attached document the boards/ modules required is AFE Module+ Docking Station?
i dont see any attachment not figures ..
Yes it needs the SOM module and the docking board .
> The UART Signals are required to interface to our controller Board for communication. IS it correct. Do we require any additional signals to be interfaced to our controller Boards. Kindly reply .
Yes correct . No the board would replace the existing host GUI .
> software package
regards.