Hi,
I'm deal with the SCI communication in F28377, and find out there isn't have receive FIFO timeout in this mcu.
Thus i need to use extra timer (like cputimer1) to implement timeout.
However there is a problem, if use two sci channel (scia & scib) for communication purpose.
Does that means i need to use two timer (cputimer1 & 2) for each sci?
If the answer is YES, then how can i avoid this problem?
Because i also need one timer to do another thing not just for sci communication.