Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8302
I use DRV8302-HC-EVM to identify a BLDC motor based pump. The pump can't be disassembled to test motor alone. I was able to run Lab02a for motor identification test, although the Rs value is stable around 0.017 Ohm, the Ls shown was very low, such as 5.138e-10, and that's obviously incorrect. So I wanted to run Lab02c for low inductance motor identification. However, I got nFAULT when the motor was locked to identify Rs. The watch window showed the following estimation state:
gMotorVars.EstState == EST_State_Rs
Once the nFAULT occurs, the remaining identification process is void. Please advise how to avoid the nFAULT from happening?