Other Parts Discussed in Thread: DRV8305, DRV8312
InstaSPIN-FOC can now be simulated and code can be generated automatically by PSIM. Several InstaSPIN examples based on TI DRV8305, DRV8312, and TMDSHVMTRPFCKIT are provided. By using this tool, you can evaluate TI's superior InstaSPIN sensorless control technology and easily incorporate it into your own product development.
PSIM provides a handy utility tool to calculate parameters required for InstaSPIN. You can simulate the entire system in PSIM and see how InstaSPIN performs in your motor control algorithm. Using PSIM's embedded code generation functionality, and with a few clicks, you can then generate the complete code automatically, upload it to an InstaSPIN enabled MCU, and start spinning the motor.
Essentially, you are able to easily test InstaSPIN with your topology + motor and then quickly progress to implementation and product development, greatly speeding up the process.
PSIM is hosting a Webinar on this topic on Thursday February 16th from 1pm-2pm EST (East Coast USA)
Sign-up here:
https://powersimtech.com/news-events/event/instaspin-webinar/