Part Number: BOOSTXL-DRV8305EVM
Other Parts Discussed in Thread: MOTORWARE
Now I am using the BOOSTXL-DRV8305EVM and the Launchpad-28069M,I want to communicate with another device via CAN bus.
the 28069M receives message from the device.
I want to add the CAN receive program to the while(1) forever loop in the motorware program.
now the CAN bus can work well in low speed mode .
Once I increase the CAN transmit speed ,it can not work.
I doubt that the CAN transmit time perhaps is less than the while(1) .
if I use the CAN receive interrupt ,whether the foc program can work well.
Thanks~