HI TI,
I wanna setup two external interrupts(XINT1 and XINT2) inside of another external interrupt (XINT3), Will it work?
Is there any documents on how to setup like this?
Also I ran into a setup problem of XINT3, somehow XINT3 ISR function is not triggered even through I applied signal into it.
XIN2_ISR and XINT1_ISR works fine, XINT3_ISR has exact same setup as XINT1 and XINT2, but it just doesn't work. I might have missed something. Please Help and take a look on my GPIO setup.
Here are my following setup, base on the ControlSuit ExternalInterrupts Example:
Hardware: F28055
interrupt void xint1WR_isr(void); interrupt void xint2RD_isr(void); interrupt void xint3CS_isr(void);
// ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.XINT1 = &xint1WR_isr; PieVectTable.XINT2 = &xint2RD_isr; PieVectTable.XINT3 = &xint3CS_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Clear the counters Xint1WR_Count = 0; // Count XINT1 interrupts Xint2RD_Count = 0; // Count XINT2 interrupts Xint3CS_Count = 0; // Count XINT3 interrupts
// Enable XINT1,XINT2 and XINT3 in the PIE: Group 1,12 interrupt 4,5 & 1 // Enable INT1 which is connected to WAKEINT: PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block PieCtrlRegs.PIEIER1.bit.INTx4 = 1; // Enable PIE Group 1 INT4 PieCtrlRegs.PIEIER1.bit.INTx5 = 1; // Enable PIE Group 1 INT5 PieCtrlRegs.PIEIER12.bit.INTx1 = 1; // Enable PIE Group 12 INT1 IER |= M_INT1; // Enable CPU INT1 EINT; // Enable Global Interrupts
// GPIO8 is input XINT1, GPIO9 is input XINT2, GPIO10 is input XINT3 EALLOW; GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; // GPIO8 GpioCtrlRegs.GPADIR.bit.GPIO8 = 0; // input GpioCtrlRegs.GPAQSEL1.bit.GPIO8 = 0; // Synch to SYSCLOUT GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 0; // GPIO9 GpioCtrlRegs.GPADIR.bit.GPIO9 = 0; // input GpioCtrlRegs.GPAQSEL1.bit.GPIO9 = 0; // Synch to SYSCLOUT GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 0; // GPIO10 GpioCtrlRegs.GPADIR.bit.GPIO10 = 0; // input GpioCtrlRegs.GPAQSEL1.bit.GPIO10 = 0; // Synch to SYSCLOUT EDIS; // GPIO8 is XINT1, GPIO9 is XINT2, GPIO10 is XINT3 EALLOW; GpioIntRegs.GPIOXINT1SEL.bit.GPIOSEL = 8; // XINT1 is GPIO8 GpioIntRegs.GPIOXINT2SEL.bit.GPIOSEL = 9; // XINT2 is GPIO9 // GpioIntRegs.GPIOXINT3SEL.bit.GPIOSEL = 10; // XINT3 is GPIO10 GpioIntRegs.GPIOXINT3SEL.all = 10; // XINT3 connected to GPIO10 EDIS; // Configure XINT1, XINT2 and XINT3 XIntruptRegs.XINT1CR.bit.POLARITY = 1; // Rising edge interrupt XIntruptRegs.XINT2CR.bit.POLARITY = 1; // Rising edge interrupt XIntruptRegs.XINT3CR.bit.POLARITY = 0; // Falling edge interrupt // Enable XINT1, XINT2 and XINT3 XIntruptRegs.XINT1CR.bit.ENABLE = 1; // Enable XINT1 XIntruptRegs.XINT2CR.bit.ENABLE = 1; // Enable XINT2 XIntruptRegs.XINT3CR.bit.ENABLE = 1; // Enable XINT3
interrupt void xint1WR_isr(void)
{
Xint1WR_Count++;
// Acknowledge this interrupt to get more from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void xint2RD_isr(void)
{
Xint2RD_Count++;
// Acknowledge this interrupt to get more from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void xint3CS_isr(void)
{
Xint3CS_Count++;
// Acknowledge this interrupt to get more from group 12
PieCtrlRegs.PIEACK.all = PIEACK_GROUP12;
}