Hi,
I have a DRV8301-69M-KIT to evaluate TI’s solution for control of a brushless DC motor. So far the kit has been used to control both the position and speed of the motor (using InstaSPIN MOTION and a quadrature encoder) - it’s some great software!
I have a question about using InstaSPIN in an environment that has some strict EMI/EMC regulations. Because of these requirements, I’m not sure that conventional “stepped”/trapezoidal commutation (2 phases high/low, 1 phase floating) will be appropriate due to the sharp changes in voltage that can have quite a large frequency response. Firstly, and correct me if I’m wrong, does InstaSPIN by default use this form of commutation? (looking at the voltage going into the motor phases in labs 12x and 13x this looks like the commutation method being used).
Is the smoothest commutation method supported by InstaSPIN SVM? (I saw Chris Clearman's comment in this post: https://e2e.ti.com/support/applications/motor_drivers/f/38/t/298166 and tried out lab 10b, but I think the waveform may still be too choppy).
And more generally, does TI have any motor solutions specifically aimed at reducing EMI from motor control?
Thanks for your advice,
Michael