Part Number: LAUNCHXL-F28027F
Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301, CONTROLSUITE, MOTORWARE
Tool/software: Code Composer Studio
Hi,
I have managed to spin the motor with BOOSTXL-DRV8301.
I went through the InstaSpin labs, found needed parameters, learned how to control the motor from the program code.
What I need now is a help with a separate PWM signal generation on a separate GPIO from DRV8301 controls. Not simultaneously with the motor but in the same program.
I tried ControlSuite examples. They work well, but when I try to merge them PLL_Setup func goes in the conflict with InstaSpin functions and I am unable to compile/link the project.
Could you please direct me to the working example or successful thread? My search has failed.
Regards,
Edward.