Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: TMS320F28377S, TMS320F28377D, LAUNCHXL-F28379D
Hallo,
i bought the TMS320F28377S LaunchPad Development Kit. And i have some Problems with the ADC conversion. To be exact i have the TMX320F28377S TPZP so i have the Silicon Revision Code B.
In the silicon errata: SPRZ422D
chapter: Advisory ADC: 12-Bit Switch Resistance
Revision B has an 2 kOhm Ron.
chapter: Advisory ADC: Random Conversion Errors
Revision B is also affected to this error.
To solve this Problem i set the acqusition time to 320 ns and the ADC to 40 MHz. The SYSCLK is running with 200 MHz. So instead of using the 75 ns from the Datasheet i have to spend much more time.
I have some questions:
Is there another revision available yet which does not have these Problems (TMS320F28377S), so the aquisition window is smaller?
How can i buy another revision (how can i be sure not to buy revision B again)?
Does the TMS320F28377D have the same Problems?
I am working at my master thesis and i have invested some time to get the C code run for the TMS320F28377S.
To i have to change my c code if i work on an other revision?
To i have to modify many things in the c code if i will work on the TMS320F28377D?
I want to digital control a LLC converter with the TMS320F28377S LaunchPad, so i have to be very fast and the ADC has to work reliable.
Any sugges
With Regards,
Jonas Hemmer