This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28055: SCI connection issue: From F28055 to F28054

Part Number: TMS320F28055

Hi TI,

  I am testing communication between F28055 and F28054M, Using example code from controllerSuit: Example_2805xSci_FFDLB_int.

Testing F28055 itself has no problem looping back data from Tx to Rx. But I want to transmit data from F28055 to F28054m, Then F28054M reads.

For the hardware connection: I connected F28055 (GPIO28/SCIRXDA and GPIO29/SCITXDA) to F28054M (GPIO28/SCITXDA and GPIO29/SCIRXDA)

So, I did following steps:

I disabled Rx interrupts ISR from F28055,( since I only need Tx)

distabled Tx interrupts ISR from F28054M

disable loop back (SciaRegs.SCICCR.bit.LOOPBKENA =0; // Disable loop back from fifo_init)

But I am not able to receive data from F28055 to F28054M, I wonder what did I missed to make them communicate to each other?

I have also attached example code below:

void main(void)
{
   Uint16 i;

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2805x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initialize GPIO:
// This example function is found in the F2805x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();
// Setup only the GP I/O only for SCI-A and SCI-B functionality
// This function is found in F2805x_Sci.c
   InitSciGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2805x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2805x_DefaultIsr.c.
// This function is found in F2805x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.SCIRXINTA = &sciaRxFifoIsr;
   PieVectTable.SCITXINTA = &sciaTxFifoIsr;
   EDIS;   // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
   scia_fifo_init();  // Init SCI-A

// Step 5. User specific code, enable interrupts:

// Init send data.  After each transmission this data
// will be updated for the next transmission
   for(i = 0; i<2; i++)
   {
      sdataA[i] = i;
   }

   rdata_pointA = sdataA[0];
// Enable interrupts required for this example
   PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block
   PieCtrlRegs.PIEIER9.bit.INTx1=1;     // PIE Group 9, INT1
   PieCtrlRegs.PIEIER9.bit.INTx2=1;     // PIE Group 9, INT2
   IER = 0x100; // Enable CPU INT
   EINT;

// Step 6. IDLE loop. Just sit and loop forever (optional):
    for(;;);
}

void error(void)
{
   asm("     ESTOP0"); // Test failed!! Stop!
    for (;;);
}

interrupt void sciaTxFifoIsr(void)
{
    Uint16 i;
    for(i=0; i< 2; i++)
    {
       SciaRegs.SCITXBUF=sdataA[i];     // Send data
    }

    for(i=0; i< 2; i++)                 //Increment send data for next cycle
    {
       sdataA[i] = (sdataA[i]+1) & 0x00FF;
    }

    SciaRegs.SCIFFTX.bit.TXFFINTCLR=1;  // Clear SCI Interrupt flag
    PieCtrlRegs.PIEACK.all|=0x100;      // Issue PIE ACK
}


interrupt void sciaRxFifoIsr(void)
{
    Uint16 i;
    for(i=0;i<2;i++)
    {
       rdataA[i]=SciaRegs.SCIRXBUF.all;  // Read data
    }
    for(i=0;i<2;i++)                     // Check received data
    {
       if(rdataA[i] != ( (rdata_pointA+i) & 0x00FF) ) error();
    }
    rdata_pointA = (rdata_pointA+1) & 0x00FF;

    SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1;   // Clear Overflow flag
    SciaRegs.SCIFFRX.bit.RXFFINTCLR=1;   // Clear Interrupt flag

    PieCtrlRegs.PIEACK.all|=0x100;       // Issue PIE ack
}


void scia_fifo_init()
{
   SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback
                                  // No parity,8 char bits,
                                  // async mode, idle-line protocol
   SciaRegs.SCICTL1.all =0x0003;  // enable TX, RX, internal SCICLK,
                                  // Disable RX ERR, SLEEP, TXWAKE
   SciaRegs.SCICTL2.bit.TXINTENA =1;
   SciaRegs.SCICTL2.bit.RXBKINTENA =1;
   SciaRegs.SCIHBAUD = 0x0000;
   SciaRegs.SCILBAUD = 0x0030; //SCI_PRD;
   SciaRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back
   SciaRegs.SCIFFTX.all=0xC022;
   SciaRegs.SCIFFRX.all=0x0022;
   SciaRegs.SCIFFCT.all=0x00;

   SciaRegs.SCICTL1.all =0x0023;     // Relinquish SCI from Reset
   SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1;
   SciaRegs.SCIFFRX.bit.RXFIFORESET=1;

}

//===========================================================================
// No more.
//===========================================================================

  • Qiang,

    That sounds like it should work, can you see GPIO25 toggling on the F28055 device?

    Secondly let us make sure your hardware connections are correct, did you connect the devices as shown below?

    ______________                      ____________
    |       F28055        |                   |    F28054M 
    |
    |                       Tx |--------------| Rx                  
    |
    |                       Rx |--------------| Tx                  
    |
    |_____________|                   |___________|

     

    Regards,
    Cody

  • Yes, I got working already. Thanks anyway!