Part Number: TMDSDOCK28335
Tool/software: Code Composer Studio
Dear All,
I have baught two nos. of TMDSDOCK28335 experimenter kit. When I am trying to connect with CCS V4 one is working fine but another one is not working. It is giving out the below error
"Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located."
What I will do now. Can anybody reply?