Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
1.
I tried building example codes but it threw an error saying - #2638 The alignment of an array element is greater than the element size
I've copied the error message -
Description Resource Path Location Type
#2638 The alignment of an array element is greater than the element size .ccsproject /buffdac_sine_cpu01 line 554, external location: C:\ti\controlSUITE\device_support\F2837xD\v210\F2837xD_headers\include\F2837xD_can.h C/C++ Problem
2. How to operate the board in Stand-Alone Mode (I referred this link but it is not working - https://training.ti.com/c2000-f28379d-dual-core-launchpad-technical-overview-demonstration-inter-processor-communications ).
Can you please suggest as to how this can be solved.
3. Even when I made a GPIO pin high it was giving a voltage of only 1.5V and the maximum voltage of DAC was also 1.5V(when 0x7FFF was given from the CCS).
Won't the pin's voltages reach nearly 5V?