This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: TMS320F28379D USB Boot Clock Source

Part Number: TMS320F28379D


In the Technical Reference Manual CAN Boot Mode Section,

It is noted that "The bit timing registers are programmed in such a way that a 100 kbps bit rate is achieved with a 20 MHz

external oscillator".

But I can't find such description in USB Boot Mode.

Should I need to connect a external oscillator to x1 when using USB Boot Mode?