This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INSTASPIN-BLDC: IQ math for Instaspin

Part Number: INSTASPIN-BLDC

Hello,

I've got some questions regarding the IQ math system used in Instaspin.

1) The controller runs by default in IQ24. Is it possible to change that to, let's say, IQ25 or IQ26? if it is possible, how is it done?

2) If all the controller runs in per unit, the maximum values you would expect would be between +-1, therefore, why not use IQ30 to increase accuracy?

3) I read some posts about moving the controller from fixed point math to float, is this possible? I've got the floating point unit enabled but I believe it is only used for external operations in the main loop.

Thanks!