Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
I found a few bugs in the external SRAM tests in emif1_16bit_asram.c for F28377S in C2000Ware 1.00.00.00:
1 - Loop variable in mem_read_write() limits external SRAM to 64K x 32 bits
mem_read_write(Uint32 start_addr, Uint32 mem_size)
{
unsigned long mem_rds;
unsigned long mem_wds;
long *XMEM_ps;
//unsigned int i; << Change to unsigned long to support external SRAM larger than 64K x 32 bits
unsigned long i;
2 - mem_data_walk only covers half of the memory covered by the other tests for a given mem_size
mem_data_walk(Uint32 start_addr, Uint32 mem_size)
{
unsigned long sram_rd;
unsigned long sram_wd;
unsigned long i;
int k;
int m;
unsigned long *XM_p;
unsigned long *XMEM_p;
XM_p = (unsigned long *)start_addr;
//for (i=0; i < mem_size; i=i+64) << need to double the mem_size to cover the same memory as the other tests because each location is tested normal and inverted
for (i=0; i < (mem_size * 2); i=i+64)
3 - Loop variable in mem_addr_walk() limits external SRAM to 64K x 32 bits
mem_addr_walk(Uint32 start_addr, Uint32 addr_size)
{
unsigned long sram_rd;
unsigned long sram_wd;
//unsigned int k; << Change to unsigned long to support external SRAM larger than 64K x 32 bits
unsigned long k;
unsigned long xshift; unsigned long *XM_p; unsigned long *XMEM_p;
The remaining are not bugs per se but useful clarifications:
4 - mem_size is the number of 32 bit words (half of the addressable size given that each address points to 16 bits)
Suggest adding a comment similar to below
#define TEST_PASS 0xABCDABCD #define TEST_FAIL 0xDEADDEAD #define ASRAM_CS2_START_ADDR 0x100000 #define ASRAM_CS2_SIZE 0x8000 // number of 32-bit words to test
5 - Remove unused timing values (these do nothing in the code and could be confusing)
#define EMIF1 0 #define EMIF2 1 #define MEM_D_WIDTH 1 // 16Bit Memory Interface #define TURN_AROUND_TIME 0 // Turn Around time of 2 Emif Clock #define RD_SETUP_TIME 0 // Read Setup time of 1 Emif Clock #define RD_STROBE_TIME 3 // Read Strobe time of 4 Emif Clock #define RD_HOLD_TIME 0 // Read Hold time of 1 Emif Clock #define WR_SETUP_TIME 0 // Write Hold time of 1 Emif Clock #define WR_STROBE_TIME 0 // Write Setup time of 1 Emif Clock #define WR_HOLD_TIME 0 // Write Hold time of 1 Emif Clock #define EXTEND_WAIT 0 // Disable Extended Wait #define STROBE_SEL 0 // Disable Strobe Mode. #define WAIT_POLAR_INV 0 #define WAIT_COUNT 0
Thanks,
Steve