This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C28346: Questions about XTIFG configuration

Part Number: TMS320C28346

Hello.

I have three questions.

1.Are following descriptions In the sprufn4a document typo?

   a."XRDACTIVE ≧ 6" is described in secction 4.1,4.2 and 4.3. 

     It is described that AR means (XRDACTIVE+WS+1) x tc(xtim).

     I think correct description when AR ≧ 6  is "XRDACTIVE ≧ 5" , isn't it ?

   b."XWRACTIVE = 2, XWRACTIVE = 4, XWRTRAIL = 2" is descrribed in Figure 14.

     I think correct description is "XWRLEAD = 2, XWRACTIVE = 4, XWRTRAIL = 2" , isn't it?

2.If the answer of question 1-b is YES, why figure 14 is described when "XWRLEAD = 2" although section 4.1, 4.2, 4.3 specifies "XWRLEAD ≧ 3" ?

3.Is my understanding correct that BCYC and BANK bit in the XBANK Register works as following flows?

     step1. Default BANK bit setting is Zone 7, and Zone 7 is accessed

     step2. When other zone is accessed , XTIMCLK cycles is inserted between access time of Zone 7 and other Zone. 

   

Regards, 

uchida-k

  • Uchida-san,

    a."XRDACTIVE ≧ 6" is described in secction 4.1,4.2 and 4.3. 

         It is described that AR means (XRDACTIVE+WS+1) x tc(xtim).

         I think correct description when AR ≧ 6  is "XRDACTIVE ≧ 5" , isn't it ?

    Your understanding is correct. This is known issue and has been registered in our system to fix in next release.

    b."XWRACTIVE = 2, XWRACTIVE = 4, XWRTRAIL = 2" is descrribed in Figure 14.

         I think correct description is "XWRLEAD = 2, XWRACTIVE = 4, XWRTRAIL = 2" , isn't it?

    That is correct. This is a typo. I'll mention this as well to fix in next release.

    2.If the answer of question 1-b is YES, why figure 14 is described when "XWRLEAD = 2" although section 4.1, 4.2, 4.3 specifies "XWRLEAD ≧ 3" ?

    These timing diagrams are just for example and have been created to go in different devices documents and in some cases  " XWRLEAD ≧ 1" is valid. User need to use correct value based on device specific constraints.

    3.Is my understanding correct that BCYC and BANK bit in the XBANK Register works as following flows?

    I will get back to you later on this one.

    Regards,

    Vivek Singh

  • Hi Vivek,

    Thank you for your reply.

    I'm also waiting for your contact about question3.

    Regards,

    uchida-k

  • Hi Vivek,

    Can I ask additional questions?

    1. Which is write trail period invalid or 0 when XWRTRAIL = 00b ?

        Write Trail Period is blank when XWRTRAIL = 00b in the table 7 at the page of 27, SPRUFN4A.

    2.Do you have something tools which detect setting invalid value to the resister ?

       For example, in case of setting XRDACTIVE = 0 although XRDACTIVE ≧ 6 according to section 4 in the SPRUFN4A.

    3.If you have something advises about following question in the previous post, please let me know.

       -> Is my understanding correct that BCYC and BANK bit in the XBANK Register works as following flows? 

       

    Regards,

    uchida-k

  • Hi Vivek,

    Do you have something update?

    Regards,
    uchida-k
  • Uchida-san,

    1. Which is write trail period invalid or 0 when XWRTRAIL = 00b ?

        Write Trail Period is blank when XWRTRAIL = 00b in the table 7 at the page of 27, SPRUFN4A.

    It is blank because XWRTRAIL = 00b is not valid configuration.

    2.Do you have something tools which detect setting invalid value to the resister ?

       For example, in case of setting XRDACTIVE = 0 although XRDACTIVE ≧ 6 according to section 4 in the SPRUFN4A.

    Sorry, we do not have tool for this.

     -> 

    3.Is my understanding correct that BCYC and BANK bit in the XBANK Register works as following flows?

         step1. Default BANK bit setting is Zone 7, and Zone 7 is accessed

         step2. When other zone is accessed , XTIMCLK cycles is inserted between access time of Zone 7 and other Zone.  

    Your understanding is correct. Please also refer section "5 Configuring XBANK Cycles" in same document for some more info on this.

    Regards,

    Vivek Singh

  • Hi Vivek,

    I understand.

    Thank you for your reply.

    Regards,

    uchida-k