Part Number: TMS320F28069
Tool/software: TI C/C++ Compiler
Hello,
customer has a problem running sometimes into ITRAP on a TMS320F28069. As it is only sometimes it is not sure if it is a compiler problem. I can send you the SW project TI internal.
Problem:
The code is running into Illegal_Isr after ca. 700ms. The problem is located with the „Timer_ISR()“.
The „Timer_ISR()“ is running from „RAML0+RAML1“. If it runs from Flash or from “RAML5” the code runs stable.
Setup:
- Compiler v6.4.2
Can you have a look into this?
Regards, Holger