Part Number: TMDSDOCK28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, SN65HVD257, RS485-FL-DPLX-EVM
Hi,
I'm using controlCARD TMDSDOCK28379D but just realized that the kit doesn't have CAN transceiver module so I can't read the differential CAN_H and CAN_L signals, however I can read CAN_TX and CAN_RX at the MCU side which are not differential. In addition, I realized that LAUNCHXLF28379D has the CAN transceiver so CAN_H and CAN_L signals are available to communicate over CAN bus. So:
1. why the CAN_RX and CAN_TX are available on the MCU but there is no CAN transceiver installed on the board?
2. Is there any CAN transceiver module that I can buy individually and connect it to my controlCARD?
Regards,
Kash