Part Number: LAUNCHXL-F28027F
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM, MOTORWARE
Hi,
I have Launchpadxl-f28027F plus boostxl-drv8305evm
I am trying to measure cpu usage in Lab5a example (from point a to point b) using Timer 2 and the project
C:\ti\motorware\motorware_1_01_00_17/sw/solutions/instaspin_foc/src/proj_lab05a.c
I want to confirm that the "timer_delta_now" value of 580, part of the cpu_time structure is the cpu usage in microseconds (usec).
My CPU Frequency is 60Mhz
Timer 2 is initialized as:
// use timer 2 for CPU time diagnostics
TIMER_setDecimationFactor(obj->timerHandle[2],0);
TIMER_setEmulationMode(obj->timerHandle[2],TIMER_EmulationMode_RunFree);
TIMER_reload(obj->timerHandle[2]);
TIMER_setPeriod(obj->timerHandle[2],0xFFFFFFFF);
TIMER_setPreScaler(obj->timerHandle[2],60);
The system is enabled and motor ID is enabled:
gMotorVars.Flag_enableSys = 1;
gMotorVars.Flag_Run_Identify = 1;
Point A = Inside while(gMotorVars.Flag_enableSys) loop
// read the timer 2 value and update the CPU usage module
uint32_t timer2Cnt = HAL_readTimerCnt(halHandle,2);
CPU_TIME_updateCnts(cpu_timeHandle,timer2Cnt);
Point B: Before "end of while(gFlag_enableSys) loop"
// read the timer 2 value and update the CPU usage module
timer2Cnt = HAL_readTimerCnt(halHandle,2);
CPU_TIME_run(cpu_timeHandle,timer2Cnt);
I am monitoring cpu_time structure continuously and I see the below data:
Thanks,
Asha