Part Number: LAUNCHXL-F28377S
Tool/software: Code Composer Studio
I'm curious if anyone with a LAUNCHXL-F28377S has been able to exceed 230,400 baud with SCI through the on-board FTDI chip to the USB? Bringing the LSPCLK up to 200Mhz gives baud rates up to 12.5 Mbaud with errors below 0.5% (including standard ones like 460,800 (0.5%), 921,600 (0.5%)). However, I can't reliably receive or transmit any data above 230,400 - it's all a garbled mess.