Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE
I designed a simple board with 28035,use 20MHz extenal crystal ,it can boot from internal flash successfully.but it can not boot from SCI,and I check all things it sames correct.when I chang the boot config pins to SCI ,send 'a',or'A',it is no any responses in the RX of the SCI,so I check clk signal no the XCLKOUT,in any conditions of reset , boot from flash,boot from SCI ,there is no any clk signal on this pin.