Part Number: TMS320F28375D
Hello,
In 32-bit async mode does a burst or dma mode exist for the EMIF?
If yes, then how do Ienable it? If I want to do a burst read from an async part?
Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28375D
Hello,
In 32-bit async mode does a burst or dma mode exist for the EMIF?
If yes, then how do Ienable it? If I want to do a burst read from an async part?
Thank you,
Hi,
System DMA can do bulk transfer via EMIF. Is that what you are looking for? Or something else? There is no inbuilt DMA inside EMIF.
Regards,
Vivek Singh
Thank you for the prompt reply on the DMA EMIF for async feature of the Delfino.
My next question is what do I have to do to initiate a DMA transfer in async mode?
Would you refer me to the specific sections of the TI datasheet for the Delfino or any related application notes for it?
I’m on the peripheral side of things relative to the Delfino; and any kind of control or acknowledgement signals that I have to provide to the Delfino are of interest to me.
Thank you for your help.