Part Number: TMS320F28375D
I have found the following two E2E threads with useful information, but I have a few followup questions for additional detail:


- What is the peak current consumption for VREFHI pin under worst case condition? What is the worst case condition for VREFHI pin? This is assumed to be during conversion.
- There are four groups of ADC. Each group has its own VREFHI. Can they be internally connected together? I think the answer is no, please confirm.
- Any layout guidance for BGA package because the requirement is :
“ Place at least a 1-µF capacitor on this pin for the 12-bit mode, ….. This capacitor should be placed as close to the device as possible between the VREFHIA and VREFLOA pins.”
Because all the pins are underneath the DSP, should the capacitor be placed on the opposite side of DSP and close to pins if double side component placement is used? Is it valid to use a single sided component placement and still have the capacitor close enough to the VREF pins?
Thanks,
Stuart