I'm looking for a maximum current the F28069 ControlCard needs to source. I've looked at sprs698f and, looking at table 5-1, the highest current I see is 245 mA. Is this for the whole control card or just the chip?
If I want to connect several GPIO pins, what amount do I add to it per pin? Also, the control card has several 5V rails (pins 96, 92, 87, 82, 77). Is the control card powered by a 5V supply or 3.3?
Thanks.