Part Number: TMS320F28069
Other Parts Discussed in Thread: UNIFLASH
We have been using 2806x piccolo devices in many products so far - right now we have an issue with the F28069. We made a board with these ICs and are trying to control different types of motors.
The ICs, board, code all work perfectly fine with different motors.
When we connect a serial port (we use an isolated RS485 driver from Analog Devices) and try to flash the program, the IC gets locked and we are not able to program the IC at all after this - we need to replace the IC to start with the board.
I have tried this with 3 devices so far - the behaviour is exactly the same and I now have 3 locked devices.
The serial port pins that I use are: GPIO28 and GPIO29.
Boot mode GPIO34 is open.
What could be the issue?
Can we somehow unlock the locked devices?
I tried Uniflash after reading a post, but even uniflash reports device is locked.