Other Parts Discussed in Thread: CCSTUDIO, TMDSHVMTRINSPIN
Hi,
I have the following problem when using GUI:
Restarting Program Model...
Initializing target : C:\ti\guicomposer\webapps\InstaSPIN_FOC_F2806xM\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
I have checked my USB port and it is configured as "TI XDS100 Channel A" and "TI XDS100 Channel B", besides LD1 of the board and control card is ON, so I guess that is not a power problem.
any solution?