Hi!
I am trying to interface a 4x4 Matrix Keypad with TMS320F28027 and displaying the identified key on 16x2 LCD.
The basic interface works fine with LCD.
Up to the single press key detection is working as expected.
In my project the second stage is to enter the number as "12.34".
Can anybody help me in writing the code for multiple parameter entries?
Thanks in advance!
Regards,
Richa