Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: ADS5560, DAC7760
In ADC datasheet:
The data is output to Launchpad and I don't know which format is for Launchpad.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Originally I was going to use embedded ADCs and DACs but I realized their specifications are not for higher frequency, for example, the SNR is tested at 100 KHz, our input signal is 10 MHz; the output is unipolar but the required outputs are both 0-10V and +/-10V. That is the reason we have to integrate stand alone ADCs and DACs although it increases a lot work.