In the SPRT720 document section 3 it shows the EMIF-1 memory space as 2Mx16, but in the EMIF section 25 of spruhm8f it shows 512MBit part... now the comment just before the chart says for devices that support the 16 bit interface...
So to be clear:
for the 28375D, if I look at the memory map it shows 0x100000 for EMIF-1 (2Mx16),
If I put a 512MBit x16 x4 part on there, that should be 8Mx16, but the address space only shows 2Mx16
What is the maximum memory that can be added to the 23875D EMIF1 x16 interface?
a 128MBit SDRAM? 32MBit SDRAM?