Part Number: TMS320F28333
Other Parts Discussed in Thread: UNIFLASH
Hi C2000 Champion
My customer use 100MZ F28232/F28335 for servo control, both work fine and servo control no problem.
Then the F28335 is replaced by F28333, as you know it is pin to pin and software compatible with F28335.
But F28333 can not be programmed through uniflash and CCS. the fail report as below:
Uniflash version is v4.1.0.
CCS is 6.1 and update to get F28333 device support.
VDD is 1.8V.
I used the flash_f28335 example to load to F28333, load fail too.
Please help to look at this problem, as customer want to MP soon.