This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335 and FPU MAC



Hi,

a efficient MAC needs two parallel MOVs. Is the F28335 FPU capable of this?

Thanks

Gustl

 

 

  • Bernhard Bauer said:

    Hi,

    a efficient MAC needs two parallel MOVs. Is the F28335 FPU capable of this?

    Thanks

    Gustl

    Two operands to the MACF32 instruction point to the source location and read the contents as part of the operation.   This can be done without stalling if the operands and source are all in seperate physical memory blocks.  These pointers automatically increment when MACF32 is combined with the RPT || instruction.

    For more details, please see the documentation for MACF32 R7H, R3H, mem32, *XAR7++ in the FPU reference guide: www.ti.com/lit/sprueo2

    -Lori