Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMS320F28379D
One questions:
From "TMS320F28379D LaunchPad Quick Start Guide", we see that there are "+5V" pins and "+3.3V" pins.
We want to ask if it means that
- the LaunchPad can be powered by these pins if it works without connection to a computer though USB
or
- the LaunchPad can provide "+5V" and "+3.3V" to other devices if the LaunchPad is connected to a computer though USB?