Part Number: TIDM-2PHILPFC
Tool/software: Code Composer Studio
Hello Sir,
Here we bought some two-phase interleaved PFC (TIDM-2PHILPFC) 390V 700W. The control card is CC2803X ISO Rev 1.3.
I turned on the SW3 on the control card so that JTAG is enabled, but the demo program from control suit still cannot get loaded. It pop up the following error :
"Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 6.0.407.3)"
It seems it cannot get connected via XDS100v1 USB debug prob.
Thank you very much in advance.