Part Number: TMS320F28069M
hello,
My application read joystick and send velocity via CAN interface. Project is modified from labs13e. Max speed of motor is 1500RPM. When I send velocity from range 0-1500 and use
gMotorVars.MaxVel_krpm = _IQ((float)speed/1000)
it seems everything works good.
But for example when application use velocity range from 0-20000(example) I need convert to max velocity 1500. So I do
float vel = (float)speed/GEARBOX;
gMotorVars.MaxVel_krpm = _IQ((float)vel)
sometimes motor run with double speed. In expressions window I see that gMotorVars.Speed_krpm show 2x bigger number then gMotorVars.MaxVel_krpm.
When I try convert with this(without cast float) so no decimal number, it is work.
float vel = speed/GEARBOX;