Other Parts Discussed in Thread: CONTROLSUITE
I recently acquired a C2000 Piccolo Launchpad. I followed the instructions found in the User's Guide but I am unable to get the serial communication working. Here's what I did:
I downloaded Code Composer Studio and ControlSuite. I installed them. I plugged the C2000 Launchpad to the PC using the USB cable. The C2000 powered up and began running the LED program that comes pre-programmed. I pressed S3 to test the temperature measurement mode (also pre-programmed) and it works. The problem is that I can't get the temperature information to display onto the PC through the USB/UART connection.
According to the instructions, when you plug the LaunchPad into the PC, windows will automatically detect the hardware and ask to install software drivers. This did not happen. According to the instructions, there should be a "USB Serial Port (COM#)" in Ports under Device Manager. You need this information configure a serial terminal app like Putty. I don't see a "Ports" in Device Manager. When I look under '"USB Serial Bus Controllers" in Device Manger, I see no entries for TI XDS100 Channel A/B, which leads me to suspect drivers were never installed.
I have read forum posts for similar problems, and their answer is always to "install CCS." I have reinstalled Code Composer Studio three times over. It's not working.
I can say that S1 switch 3 is in the up position. Jumpers are on JP1, JP2, JP3 and both power LEDs are on. S4 is in the Up position. In short, I don't think there's a hardware issue.
The link to the user manual is www.ti.com/.../spruhh2a.pdf