Thank you very much.
One more thing, I would like to change DC voltage input in PR902 schematic,
We want to input and output voltage. Such as DC input 24V, DC output 5v, 3.3v, -15v.
I am going to use all the parts as it is.
I use all of parts that like PR902 schematic.
I think I need to change the T1(GA3544-BL), and increase resistors in primary. Isn't that right?
Or should I find another circuit?
Help would be appreciated.
Regards.