Part Number: TMS320F28377S
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hi,
1. I'm trying to implement Serial communication between PC and MCU(TMS320F28377S). I tried the examples in Control Suite such as SPI, SCI, "USB_dev_bulk" but none of them worked.
What are the changes that I have to make in the program for it to work.
2. I read on the forum that " the LaunchPad uses a 10MHz external oscillator and the example in controlSUITE is designed for the controCard which uses a 20MHz external oscillator " .
So what changes should I make for this.
Thanks & Regards,
Shiva