Part Number: TMS320F2809
Other Parts Discussed in Thread: CONTROLSUITE
In order to check the errata chip for a new bought block of microcontrollers TMS320F2809, I've tried to understand the chip revision from the device markings, to check, then, it on the sprz171r document the known issues(if i'm not wrong it is the last revision of the errata chip).
The full lot trace code string printed on the chip is CC-6ACD25W, so I think that the chip revision is "C" (the second "c" to be precise, since the first it should be the "assembly site code", that can be one or two characters).
Now, searching for "C" revision for the 2809 in the document mentioned before, it doesn't give any results.
So the questions are:
- Which is the actual silicon revision and which part of the silicon errata document should I check?
- Which version of flash API should I use for writing the flash memory, from the program running on the microcontroller?
- Where can I find the flash API library, I haven't found it neither in Controlsuite nor in the 2809 page of TI site (there is only a reference that says that the product is active but it doesn't give a link to download).
In attachment the microcontroller's photo.
Thank you in advance.