Part Number: TMS320F28075
Hello,
PZP package does not have some PWM output pin such as PWM1 and PWM4, but I know actual PWM module is in PZP package. Now I want to know if the user can set the register of PWM1 and PWM4 module for PZP package parts. For example, can the sync output be disabled for PWM1 and PWM4 module of PZP package?
Now INPUT5 is used as a TRIP for PWM and the pin is pull-up externally. On this condition, EXTSYNCIN1 is connected to PWM7 through PWM1 or PWM4, so PWM7 does not have correct sync operation. So, I want to disable the sync toutput from PWM1 and PWM4 even if PZP package does not have PWM output signal.
From the test, PWM1 and 4 module register can be set for PZP package, but I want to assure this how to use is no problem or not, just in case.
Regards,
Furuya