Part Number: TMS320F28055
Other Parts Discussed in Thread: CONTROLSUITE
I use DPlib Sine analyzer. In graph, I attached, sine wave that input in Sine analyzer. Sine analyzer invoke at 10000 Hz. Threshold is 0.1. Sine fetching frequency at 80000 Hz.
Problem is a not stable result of out parameters. For example, the frequency constantly jumps between bandb 98 - 102 Hz. Vrms and Vavg have same problem. This introduces instability into the operation of the feedback current loop.
How can I solve this problem?
Dlogger
It's my oscilloscope viewing sine