Part Number: TMS320F28379D
Other Parts Discussed in Thread: DRV8301, DESIGNDRIVE
Hi guys,
I want to implement low voltage brushless motor control with absolute encoder (with SSI or BISS interface) using F28379. I know that the position manager module of 28379 can read absolute encoder with SSI/BISS interface (I read it with IDDK module before) So my questions are:
1) Can I do it with F28379D LaunchPad Development Kit + DRV8301 Motor Drive BoosterPack? Do they work together? Or do you have better suggestions?
links are here: http://www.ti.com/tool/launchxl-f28379d and http://www.ti.com/tool/boostxl-drv8301
2) If I use these boards, do I need an external circuitry to interface SSI/BISS encoders? If yes,Ii would be much appreciated if you could suggest me a small commercial card.
Regards,
Hakan