Other Parts Discussed in Thread: DRV8301, UCC27211
Hello,
We have developed permanent magnet brushless/sensorless 3-phase motors and have used many of the DRV301 kits. While the motor does run the mosfets continue to blow up. Input voltage is 48 VDC, output capability of the motor is 4.4 Kw (6 HP). We can run these motors using Kelly controllers but do not want to go into production with these. Our software is important and we use code composer perfectly.
Is there a TI controller that we can use? I understand that the DRV8301-HC-Kit states that it can handle 60 V in; 82.5 Amps full scale range. Does this controller really have more amperage handling capability than the DRV8301-69M-Kit?
Please refer me to the correct TI part number if the HC is not what we want. We have been through 6 of 69M kits and right around 30 Amps the mosfets blow up.
Kindest regards,
Jon Harms, CTO; MagLev Energy, Inc.