Part Number: TMS320F28377D
Other Parts Discussed in Thread: TMS320F28069, SFRA, CONTROLSUITE, POWERSUITE
Tool/software: Code Composer Studio
Hello TI engineer!
I am currently studying Grid Connected Inverter Design Guide! I want to use 28069 instead of 28377, because the 28377 is High-end. I developed inverter products do not need!I transplanted the existing TMS320F28377 program to TMS320F28069 is feasible?I would like to continue using 28377 powerSUITE Solution Adapter and SFRA,Because I think this platform is very powerful.I'm just going to use TMS320F28069.I want to speed up the development process!(It would be best if I could use 28035)Could you tell me if this is feasible?Thanks very much! (Link:C:\ti\controlSUITE\powerSUITE\v_1_07_00_00\HV_1PH_DCAC\f2837x\gridconnectedinvlclfltr)