This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8302-HC-C2-KIT: re-load original set up

Part Number: DRV8302-HC-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC

Team,

I have a customer who can't get the module to operate while recreating the example in controlSuite working, he is using CCS vr. 7; ControlSuite & 28035 Piccolo DIM Module.  He wants to load the original software back into the EVM.

DRV8302-HC-C2-KIT (Rev. D)

Can you outline the steps?

Regards,

Aaron

  • Hi Aaron,

    Which example are you referring to? The .out loaded onto the F28035 device that works out of the box with the InstaSPIN-BLDC GUI is no longer supported. We suggest loading a new .out from another example project to continue evaluating the product.

    Sean
  • Aaron & Sean,

    I have the DRV8302-HC-EVM Rev D Board and a Teknic M-1230P-LN-04K PM Motor. I want to load code back into F28035 Dimm and have it work with the provided InstaSpin GUI. A different engineer worked with this EVM sometime ago. He is no longer with the company and I now need a motor and a simple PC-based interface to control the speed of a motor for testing here in the lab (very light loading). Originally this looked like a quick solution, but now I'm not so sure. You don't support the code I am trying to run any longer and suggested using a different project. What would you suggest? Is there an upgraded version that will accomplish this goal?

    Joe

  • Please check this directory in ControlSuite: C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\GUI_project_InstaSPIN_BLDC

    That is probably the project you are looking for

    Sean