Part Number: TMS320F28022
Tool/software: TI C/C++ Compiler
CCS v6, Piccolo 28022, Win7 SP1 32bit.
I am debugging my C code, so I have the .text section located in ram.
It is getting to big to totally fit, so I have moved some debugged routines to flash. That seems to be working OK.
The processor does not have a FPU, so I am using the software floating point routines like pow, sin, etc... from the RTS lib 'RTS2800_ml.lib', and would like to move those routines to flash also.
I tried to place a #pragma CODE_SECTION in the math.h file, but it is still showing up in the text section.
Questions:
1) What is the easiest way to simply tell the linker I wish to place the those RTS routines in FLASH either piecemeal or in total?
2) Must I recompile the RTS code in order to get linker to locate those routines in FLASH. (I would think I should not have to do this.)
Thanks, Mark.