Part Number: TMS320F28062
Hi C2000 Team,
In the DS of the F28062 is recommended (page 85):
"Unused ADCIN pins that are multiplexed with AIO function should not be directly connected to analog ground. They should be grounded through a 1-kΩ resistor. This is to prevent an errant code from configuring these pins as AIO outputs and driving grounded pins to a logic-high state."
What is the root cause for this behavior? What is the detailed Issue (higher current, software stall…)? What could happens if we not following this recommendations? Is there any risk analysis done? Background is that 1kOhm resistors need some space at the PCB and needs also a costlier routing. If it riskless possible to waive this?
Thanks!