Part Number: TMS320F28027
Hi C2000 champs,
My customer has a question about Flash pipeline.
After the function call, the Program Counter will jump to the address of the called function.
If that address is even or odd, will Flash pipeline miss prefetch?
When making a mistake, how many words are offset by the maximum?
My customers have a issue that the control becomes unstable if the address of the function have 1 offset address.
This means,
1 offset : unstable
2 offsets: stable
3 offsets: unstable
4 offsets: stable...
I believe she has other issue. But first let me check from here
Regards,
Shinji Ueda