This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/F28M35H52C: epwm changes frequency when booting from flash

Part Number: F28M35H52C

Tool/software: Code Composer Studio

Hello,

I have an issue with my microcontroller. I'm trying to adjust the frequency of the pwms to run at 2kHz  by setting:

  InitFlash();

	EPwm2Regs.TBCTL.all = 0; 			// clear all bits in TBCTL
	EPwm2Regs.TBCTL.bit.CLKDIV = 0;  	// CLKDIV = “div by 1”;
	EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; 	// HSPCLKDIV = “div by 1”
	EPwm2Regs.TBCTL.bit.CTRMODE = 2;  	// count mode = up-down mode
	EPwm2Regs.AQCTLA.all = 0x0006; 		// ZRO=set; PRD=clear
	EPwm2Regs.TBPRD = 37500;    		// 2 kHz PWM frequency
	// TBPRD = fcpu / (2* fpwm * CLKDIV * HSPCLKDIV)
	// TBPRB = 150 MHz / (2 * 2 kHz * 1 * 1)

but they run at a different frequency. When I disconnect the card from ccs and reconnect it to run from flash it runs at the correct 2kHz frequency. Does anyone have an idea where the problem might be? 

The switches on the card for BOOT are as follows

1-down

2-down

3-down

4-down