Part Number: LAUNCHXL-F28027F
Tool/software: Code Composer Studio
Hi,I m trying to run 3 phase interleaved buck converter with launchxl-28027f. Could you please provide me the program/files for it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-F28027F
Tool/software: Code Composer Studio
Hi,I m trying to run 3 phase interleaved buck converter with launchxl-28027f. Could you please provide me the program/files for it.
Gannamraju,
We have not yet implemented any reference designs or kits using the multi-phase buck topology. In principle, you could look at the buck converter booster pack and supporting code, which implements two independent buck converters:
http://www.ti.com/tool/boostxl-buckconv
For a three phase interleaved design you will have to code the PWMs differently (see attached example), and implement current balancing if that is required.
Regards,
Richard
;
Hi i am trying to generate 3 phase interleaved buck converter.I want 120 degree phase shift.i am not generating for synchronous buck converter.Richard Poley said:Gannamraju,
We have not yet implemented any reference designs or kits using the multi-phase buck topology. In principle, you could look at the buck converter booster pack and supporting code, which implements two independent buck converters:
http://www.ti.com/tool/boostxl-buckconv
For a three phase interleaved design you will have to code the PWMs differently (see attached example), and implement current balancing if that is required.
Regards,
Richard
(Please visit the site to view this file)
i want pwm1:epwm2A
PWM2:epwm2B
Pwm3:epwm3A.
My program is shown below.Could you check whether the logic is correct?
COULD YOU PLEASE HELP ME
THANKYOU
EPwm1Regs.TBPRD = 600; // Period = 601 TBCLK counts
EPwm1Regs.CMPA.half.CMPA = 200; // Compare A = 350 TBCLK counts
EPwm1Regs.CMPB = 200; // Compare B = 200 TBCLK counts
EPwm1Regs.TBPHS = 0; // Set Phase register to zero
EPwm1Regs.TBCTR = 0; // clear TB counter
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Phase loading disabled
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLK
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm1Regs.AQCTLA.bit.PRD = AQ_SET;
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm1Regs.AQCTLB.bit.PRD = AQ_CLEAR;
EPwm2Regs.TBPRD = 600; // Period = 601 TBCLK counts
EPwm2Regs.CMPA.half.CMPA = 200; // Compare A = 350 TBCLK counts
EPwm2Regs.TBPHS = 400; // Set Phase register to zero
EPwm2Regs.TBCTR = 0; // clear TB counter
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Phase loading disabled
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // TBCLK = SYSCLK
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm2Regs.AQCTLA.bit.ZRO= AQ_SET;
EPwm2Regs.AQCTLA.bit.CAU= AQ_CLEAR
Gannamraju,
You will need to implement something similar to the waveforms I sent you, even if you are not driving synchronous buck converters. You cannot do this with two PWM modules, because each module has only two comparators against which edges can be placed. You will require three separate PWM modules, with time-bases synchronised as shown in the diagram.
To illustrate the limitation, your code switches both PWM1A and PWM1B on the period event, so it cannot be correct in a 3-phase application.
Regards,
Richard